AXIS#.SAFEPARAM.SLP_#.FAULTREACTION

Description

Indicates the safety function activated when the Safely Limited Position (SLP) safety function is faulted. The parameter uses one of the following values:

Value Description

1

STO

2

SS1 Instance 1

3

SS2 Instance 1

 

Parameters Editor showing the Fault Reaction options circled

Context

For complete SLP information refer to SLP (Safely Limited Position).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

1, 2, 3

Default Value

1 (STO)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLP_1.FAULTREACTION

316ch

07h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLP_2.FAULTREACTION

316dh

07h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLP_3.FAULTREACTION

316eh

07h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLP_1.FAULTREACTION

326ch

07h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLP_2.FAULTREACTION

326dh

07h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLP_3.FAULTREACTION

326eh

07h

Unsigned8

-

-

Read/Write

No